EEO#.LINES

Description

Sets how many lines are output for one revolution of the source feedback. When configured to output CW/CCW or Step/Dir signals (EEO#.MODE 1 or 2) you will get 4 times this value of pulses per revolution.

Examples

Code

This will set the number of EEO2 lines to 8096.

-->EEO2.LINES 8096

Context

For more information see Output - Encoder Emulation.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 16777215
Default Value 1024
Data Type Integer
See Also  
Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

EEO1.LINES

4600h

02h

Unsigned32

-

-

Read/Write

No

EEO2.LINES

4601h

02h

Unsigned32

-

-

Read/Write

No

EEO3.LINES

4603h

02h

Unsigned32

-

-

Read/Write

No

EEO4.LINES

4606h

02h

Unsigned32

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

EEO1.LINES

32005

7D05

Unsigned32

Read/Write

-

EEO2.LINES

32006

7D06

Unsigned32

Read/Write

-

EEO3.LINES

32007

7D07

Unsigned32

Read/Write

-

EEO4.LINES

32008

7D08

Unsigned32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

EEO1.LINES

32005

Unsigned32

Read/Write

-

EEO2.LINES

32006

Unsigned32

Read/Write

-

EEO3.LINES

32007

Unsigned32

Read/Write

-

EEO4.LINES

32008

Unsigned32

Read/Write

-